Codewarrior installation on Windows 7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior installation on Windows 7

4,222 Views
Southernboy
Contributor I

Dear Freescale,

 

I've been running Codewarrior with no problems for the last 3 years or so, using Windows XP. I have a dongle.

My system has been upgraded and I am now using windows 7. I initially tried to install the software, but this failed on the install. I then installed Windows 7 ultimate and tried again in XP mode.

The installation worked ok, and the dongle software installed ok (HASP). The FlexLM can detect when the dongle is installed.

When I run the diagnostics for the FlexLM, the message "Terminal Server remote client not allowed" is appearing.

When I run the codewarrior I also get the same message.

Please could you suggest what I am doing wrong?

Thanks in advance.

Labels (1)
0 Kudos
Reply
3 Replies

2,018 Views
Southernboy
Contributor I

Hi, I forgot to mention I'm using Codewarrior V6.3.010

 

Thanks

0 Kudos
Reply

2,018 Views
ck_max
Contributor I

Hi,

 

I use CW6.2 in Win7RC too. They(v7.1 and v6.2) are both unstable(crash often) but usable.

 

Regards,

Max. 

0 Kudos
Reply

2,018 Views
ck_max
Contributor I

Hi,

 

I'm using  win7rc with code warrior 7.1 for weeks. It seems no problem of this.

You can try to run the installer as administrator.

 

Regards,

Max. 

0 Kudos
Reply