Combining s19 files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Combining s19 files

2,177 Views
skyguy
Contributor III
Various older posts refer to a 'burner.exe' utility program and a 'hexfile' command in the CodeWarrior linker.  Neither of these seems to exist in the version of CodeWarrior I'm using (7.1, on Windows Vista).  Does anyone know what happened to these, or can anyone suggest an alternative tool?  I need to combine two programs into one production load file.
Thanks,
Rick
Labels (1)
0 Kudos
Reply
1 Reply

1,142 Views
BlackNight
NXP Employee
NXP Employee

Hello,

the burner is part of the CodeWarrior for S12 or for MCU (S08 and ColdFire V1).

I suggest you download the free special edition version from here:

http://www.freescale.com/lgfiles/devsuites/HC08/CW_MCU_V6_3_SE.exe?WT_TYPE=IDE%20-%20Debug,%20Compil...

 

The burner.exe is located in the prog folder.

 

BK

0 Kudos
Reply