Codewarrior and Eclipse.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior and Eclipse.

1,465件の閲覧回数
infoclog
Contributor III

I downloaded the eclipse version of Code warrior and wanted to know if it will work with my controller MPC5604B. If yes, why do we have a parallel development for CodeWarrior IDE?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,181件の閲覧回数
CrasyCat
Specialist III

Hello

 

According to the product page

    http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&tid=CWH

 

CodeWarrior for MCU Eclipse v10.1 supports following Qorivva processors:

 

Qorivva MPC56xx

  • MPC560xP: Qorivva 32-bit MCU for Chassis Applications
  • MPC567xK: Qorivva 32-bit Microcontroller for ADAS Applications
  • MPC564xL: Qorivva 32-bit MCU for Chassis and Safety Applications

 

So MPC5604B does not seem to be supported there.

 

CrasyCat

0 件の賞賛
返信