CodeWarrior 5.6.1 MCF5271 - Compiler Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior 5.6.1 MCF5271 - Compiler Question

2,632件の閲覧回数
theJoel
Contributor III
Hi all,

I'm running CodeWarrior 5.6.1.1570 with a ColdFire 5271.

I've been trying to review and optimize our application, running on a MCF5270. I'm finding when we dereference a pointer to a structure, or equate structures, the compiler generates code larger and slower than we would like.

Eg.
compiling this:
*(InternalPVPoint*)ptr1 = *(InternalPVPoint*)ptr2;
generates this:
    movea.l 4(a4),a1
    movea.l (a4),a0
    move.b (a0),d1
    move.b d1,(a1)
    move.b 1(a0),d1
    move.b d1,1(a1)
    move.b 2(a0),d1
    move.b d1,2(a1)
    move.b 3(a0),d1
    move.b d1,3(a1)

The compiler obviously knows the structure is 4 bytes, and the processor is a 32-bit ColdFire..

SO: why did CodeWarrior not generate a single longword move? How can I affect the compiler output to do this?

this example is perhaps a bit overly complicated as the type InternalPVPoint is a union containing bitfields:
typdef union tagInternalPVPoint
{
    struct
    {
        uint_32 TYPE     : 10;
        uint_32 INSTANCE : 22;
    }
    uint_32 RAW;
} InternalPVPoint;


However, using even simple structures:
typedef struct tagMyStruct
{
    uint_32 fourbytes;
} MyStruct;

typedef struct tagOtherStruct
{
    uint_32 otherfourbytes;
} OtherStruct;

void foo()
{
    MyStruct*     first;
    OtherStruct*  second;

    *first = *((MyStruct*)second);
}

produces this:
     move.w   (a0),d1
     move.w   d1,(a1)
     move.w   2(a0),d1
     move.w   d1,2(a1)


Why just do word moves?

But maybe this example is too artificial. Anyways, can anyone explain the compilers behaviour here, and how to write optimal code in these situations?

Where is the trade-off for calling an optimized (inline?) memcpy function?

--
Alban Edit: CW version number and core in subject line.

Message Edited by Alban on 2007-03-27 11:36 PM

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,182件の閲覧回数
CrasyCat
Specialist III
Hello
 
If you are suggesting an improvement in the code generated by the compiler I would suggest you to submit a service request  for that.
 
To log the issue please go to following URL:
    http://www.freescale.com/TechSupport
and click on "Submit a service request"
 
Make sure to attach source code reproducing the superfluous code and explain what you are looking for.
 
CrasyCat
0 件の賞賛
返信

1,182件の閲覧回数
theJoel
Contributor III
Thanks CrasyCat, but I don't think I need to request a compiler change.

Is it not expected a compiler for a 32-bit architecture would be able to move 4-bytes at a time??

How can I write C code to do this?


Joel.
0 件の賞賛
返信