Code Warrior Targeted compilation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior Targeted compilation

ソリューションへジャンプ
2,114件の閲覧回数
Geek19
Contributor III

I have a test code that compiles and links with no problem when I target RAM using the evaluation CW 2.7 on Windows 7 and EVAL board MPC5554. As I choose the Flash as my target the compile and link process results in several Compiler errors, warnings as well as Linker errors. Could you please explain this and show me how to resolve this matter.

Thanks;

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,503件の閲覧回数
Geek19
Contributor III

I got the answer for this question! And the answer is the P&G debugger that accompanies the Evaluation board was not loading the right *.elf  for the compiled code even though it was being launched by CW software! Basically the CW does not communicate the name of the CURRENT *.elf with the P&G debugger. The user shall pay attention and set this as needed.

Thanks;

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,504件の閲覧回数
Geek19
Contributor III

I got the answer for this question! And the answer is the P&G debugger that accompanies the Evaluation board was not loading the right *.elf  for the compiled code even though it was being launched by CW software! Basically the CW does not communicate the name of the CURRENT *.elf with the P&G debugger. The user shall pay attention and set this as needed.

Thanks;

0 件の賞賛
返信