Code Warrior TAP Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior TAP Problem

2,248 Views
jeremy_henderso
Contributor I

We just ordered and received two CWH-CTP-BASE-HE CodeWarrior Tap devices and one appears to be malfunctioning. Sometimes on power up, the TX/RX light flashes orange and never recovers. Other times it powers up and the TX/RX light flashes green, but after some time it eventually stops flashing and stays solid green and Windows displays the message in the attached screenshot. In both cases there is no serial output on the terminal.

 Our other CWH-CTP-BASE-HE TAP device appears to work fine on the same machine with the same USB port and cable.

0 Kudos
Reply
1 Reply

2,117 Views
Pavel
NXP Employee
NXP Employee

Try to reinstall CodeWarrior TAP driver. See the readme.txt using the follow path:

C:\Freescale\CW4NET_v2019.01\Common\CCS\drivers\usb

 

Test your CodeWarrior TAP using Ethernet connection. See the 1.2.3.2 of CodeWarrior TAP User Guide:

https://www.nxp.com/docs/en/user-guide/CWTAPUG.pdf


Have a great day,
Pavel Chubakov

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply