Code Warrior TAP Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior TAP Problem

2,211件の閲覧回数
jeremy_henderso
Contributor I

We just ordered and received two CWH-CTP-BASE-HE CodeWarrior Tap devices and one appears to be malfunctioning. Sometimes on power up, the TX/RX light flashes orange and never recovers. Other times it powers up and the TX/RX light flashes green, but after some time it eventually stops flashing and stays solid green and Windows displays the message in the attached screenshot. In both cases there is no serial output on the terminal.

 Our other CWH-CTP-BASE-HE TAP device appears to work fine on the same machine with the same USB port and cable.

0 件の賞賛
返信
1 返信

2,080件の閲覧回数
Pavel
NXP Employee
NXP Employee

Try to reinstall CodeWarrior TAP driver. See the readme.txt using the follow path:

C:\Freescale\CW4NET_v2019.01\Common\CCS\drivers\usb

 

Test your CodeWarrior TAP using Ethernet connection. See the 1.2.3.2 of CodeWarrior TAP User Guide:

https://www.nxp.com/docs/en/user-guide/CWTAPUG.pdf


Have a great day,
Pavel Chubakov

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信