Cannot start license server , server lmgrd is not started

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot start license server , server lmgrd is not started

3,526 次查看
Vishwanath_RR
Contributor I

Hi There

 

I have installed Free scale code warrior for coldfire v7.1 in my machine and  unable to connect to license server.find the attached error. THe license .dat files are verified , the host is same as in server.

 

Could you suggest me in this regards

R.R.Vishwanath

 

code-warrior.jpg

Message Edited by t.dowe on 2009-10-29 09:12 AM
标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

2,383 次查看
J2MEJediMaster
Specialist I

A floating license problem. Those are not easy to solve. I recommend that you file a service request to get the support that you need. Click here to go to the service request page. For the Category Option choose Technical Request, and for the Topic option select license issues.

 

Before you file the service request, make sure that you can answer the following:

 

1) If the license server is using the default ports (27000–27009), does your LAN allow them?

2) Are other systems experiencing the same problem, or just this one?

 

---Tom

Message Edited by J2MEJediMaster on 2009-10-29 09:16 AM
0 项奖励
回复

2,383 次查看
Vishwanath_RR
Contributor I

YesTom

 

The other system is facing the same problem too, but a different error, see the attachment

Tried with 3 port no.s , but still the same error.

 

keyNotFound.jpg

Message Edited by t.dowe on 2009-10-29 09:11 AM
0 项奖励
回复

2,383 次查看
J2MEJediMaster
Specialist I

I'd check to see what is different for the LM_LICENSE_FILE environmental variable between the two machines. One is seeing the license server but not getting a license key and the other just flat-out is not seeing the server. As I suggested, file a service request, and present the information you gave me here to them. Learn how to generate error logs from the server, as that helps track down whether the network or the server is having issues. And be prepared to tangle with the network IT guy. The most difficult floating license problems I have dealt with is where the IT people insist the network is not blocking the ports you are using, and it turns out that they are.

 

---Tom

Message Edited by J2MEJediMaster on 2009-10-30 09:05 AM
0 项奖励
回复

2,383 次查看
Vishwanath_RR
Contributor I

Yes Tom

 

I filed a request and awaiting their reply

0 项奖励
回复