CW6.7 - MPC8560 - Flash Programmer: CCSProtocolPlugin::Could not connect

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW6.7 - MPC8560 - Flash Programmer: CCSProtocolPlugin::Could not connect

7,585 次查看
typhon14
Contributor I
Hi all!
I used the Codewarrior for MPC8560, it worked well utill last month, but it dosen't now.
Error message is as below;
 
Using Algorithm: intel16x2j3.elf
 

======================================================================
=== Target Configuration Settings
=== Connection:    CodeWarrior Ethernet TAP
=== Target Processor: 8560
=== Target Init File: C:\Program Files\Freescale\CodeWarrior PA V8.7\PowerPC_EABI_Support\Initialization_Files\PQ3\8560ADS_RevA_init_CSJ.cfg
======================================================================
Connecting...
Flash Programmer: CCSProtocolPlugin::Could not connect to the requested core core #0.
Timestamp:  Thu Oct  4 10:57:22 2007
 
What's wrong with it?
 
Our environment is as below;
CW version : 8.7
Host OS : Windows XP(Use the dongle key)
H/W tool : Ethernet TAP
CPU : MPC8560
 
Please, give me a answer
Thank you in advance!
 
Best Regards,
Benson.
 
--
Alban Edit: Please always include FSL Part Number + CW Version in Message Subject line. Also a meaningful subject line was created.



Message Edited by Alban on 2007-10-04 09:39 AM
标签 (1)
标记 (1)
0 项奖励
回复
6 回复数

1,999 次查看
Black
Contributor I

What did you change in your working setup before this problem has occurred? This CCS connection problem can have various causes.

Please use a known working standard evaluation/development board for connection testing if available. Please debug the Debug Version of a stationery project (created with CW New project wizard) with "Verify Memory Writes" checked and board .cfg file selected in the EPPC Debugger Settings panel of this project target in order to test your Ethernet TAP connection and CodeWarrior settings. Please use the default Ethernet TAP settings and add the static IP Address of the EthernetTAP in the remote connection settings. If still not working you can check the "Force shell download" (please do not use this option afterwards).

Then if still not working, please review the actions described in the Ethernet TAP "Troubleshooting" section of the CodeWarrior Ethernet TAP User's Guide.pdf. If still unsuccessful you may rewrite the Ethernet TAP firmware as described in the CodeWarrior Ethernet TAP User's Guide.pdf (located in CodeWarrior 8.7 installation folder\Help\PDF) chapter Reprogramming the Ethernet TAP Probe Firmware Image.

You can also check if you have the release version of CodeWarrior PA 8.7 build 70321 (CodeWarrior menu, Help->About...->Installed Products).

I hope this helps,

Black

0 项奖励
回复

1,999 次查看
typhon14
Contributor I
Hi all!!
 
I found a cause of the problem. It was the bad target cable. :smileysad:l
 
Thank you for supporting!
 
Best Reagads,
Benson
 
0 项奖励
回复

1,999 次查看
cimbom
Contributor I
Hi,

I have the same problem every time by the first using the CodeWarrior after I started my PC.
I push the "debug" button to debug my code but I get the error message "CCSProtocolPlugin::Could not connect".
My solution is to use an example projekt from "Processor Expert EXAMPLES Stationery".
There are a program named LED. If I use this program I can debug it without an error message. And after this I can debug my own program. Why does this happen?
And this happens every time I shut down the PC and starts it again.
What do I have to adjust in CodeWarrior?

Thanks
 


Message Edited by cimbom on 2008-01-10 09:51 AM
0 项奖励
回复

1,999 次查看
Black
Contributor I
It seems I have posted my message in the same time with J2MEJediMaster:smileywink:
0 项奖励
回复

1,999 次查看
J2MEJediMaster
Specialist I
Not a problem. Thanks for the assist! :smileyhappy:

---Tom
0 项奖励
回复

1,999 次查看
J2MEJediMaster
Specialist I
I'd need more information before I can even attempt an asnwer.

1) Is the setup still the same? Are you using the same PC, cable, and target board?

2) Did something change after the time the arrangement worked? Did you:
  a) Add software (new ethernet driver or application)?
  b) Change the hardware (new EtherTAP, new network card)?
  c) Did the network you use to connect to the EtherTAP change in any way?

3) Could something have happened to the dongle? Go to the IDE's Help menu and check if all of the licensed modules are active. (Help | About CodeWarrior, then click on Installed Products.)

---Tom


Message Edited by J2MEJediMaster on 2007-10-04 10:17 AM
0 项奖励
回复