Codewarrior for Coldfire 7.0 wont run a Coldfire 6.4 project or new project created with 7.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior for Coldfire 7.0 wont run a Coldfire 6.4 project or new project created with 7.0

2,524 Views
Technoman64
Contributor III
I can not get version 7.0 for coldfire to work with a project that was created with version 6.4. I can open Version 6.4 load the project, write to FLASH on MCF52223 mcu and debug, run no problems.
 
If you try using 7.0 on an older project MAKE sure you back it up! Thankfully I did!
 
After many hours of messing around I finally got verion 7.0 to write toi FLASH, still not sure it iswriting correctly though as nothing seems to work write when running from FLASH. I would have thought a working project from version 6.4 would not have caused me grief. Something has changed though.
 
Anyone else had a chance to work with Version 7.0 and program internal FLASH mcu?
 
Just wondering if its just me or?
 
 
Labels (1)
0 Kudos
Reply
1 Reply

737 Views
Technoman64
Contributor III
I gave up and purchased Code Sourcery G++ IDE for Coldfire. Works great after fixing thier standard linker script.
0 Kudos
Reply