CW??? for PPC - RPM'S & Install

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW??? for PPC - RPM'S & Install

2,203件の閲覧回数
bernesbyj
Contributor I

Long Time user on Mac/Windows new at Linux/PPC.

I tried to install on Linux host, I get the following Errors, after completing the installing 100% of the files in progress bar.


1) "chmod:/usr/local/Freescale/CodewarriorIDE/Codewarrior/Cross_Tools: No such directory or file"

2) "rpm:"/root/drop/disk1/mtwk-lnx-powerpc-linux-gnuspe-gcc-3.4.3-e500-glibc-2.3.3-spe-0.28.i686.rpm" No such directory or file"

Do I have to do a reinstall, since the RPM's did not install?

Thanks

James

--
Alban Edit: Please always state CW version and target in subject line.

Message Edited by Alban on 2007-03-28 08:40 PM

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,130件の閲覧回数
Voxan
Contributor III
Hi James,

could you perform a "rpm -qa | grep mtwk" command??
it should return the list of installed GCC tool chains.

FYI: the GCC tool chains are installed under /opt/mtwk/usr/local/ folder.
BTW what CodeWarrior version are using using ??

Hope this helps...

Best Regards
0 件の賞賛
返信