CW for MPC55xx V2.7 flash programming error 14

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CW for MPC55xx V2.7 flash programming error 14

跳至解决方案
2,162 次查看
MPCMpy
Contributor II

I use the freescale MPC5554EVB with the PE's CABPPCNEXUS,it can download the (CodeWarrior_Examples) to the RAM.When the examples was downloaded to the flash an error appeared.(error 14,just like the picture in the attatchment)!And after put the MPC5554EVB into the icebox for minutes,the examples can be dowloaded to the flash once!Who can tell us what's wrong with this! Is the flash damaged?I  downloaded the examples to the flash ROM only 10 times.By the way,whether the PC OS isWindows XP or WIN7,the error always appears.

Thanks

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,312 次查看
MPCMpy
Contributor II

The heatsink of the triode dropped. I have installed it .Now, it works well.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,313 次查看
MPCMpy
Contributor II

The heatsink of the triode dropped. I have installed it .Now, it works well.

0 项奖励
回复
1,312 次查看
MPCMpy
Contributor II

I use the freescale MPC5554EVB with the PE's CABPPCNEXUS,it can only download the (CodeWarrior_Examples) to the external RAM.When the examples was downloaded to the flash an error appeared.(error 14,just like the picture in the attatchment)!And download it to the internal RAM it is also wrong!After put the MPC5554EVB into the icebox for minutes,the examples can be dowloaded to the flash once!Who can tell us what's wrong with this! Is the flash damaged?I  downloaded the examples to the flash ROM only 10 times.By the way,whether the PC OS isWindows XP or WIN7,the error always appears.

Thanks

0 项奖励
回复