CW MPC55XX in Win7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,025件の閲覧回数
TimMilliken
Contributor II

The installer tells me that I have an unsupported OS, ask do I want to continue, I chose yes, but nothing happens. Can someone direct me to a solution please, no fun working on laptop only..

 

Tim

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,031件の閲覧回数
TimMilliken
Contributor II

Also it a version of Win 7 from an MSDN subcription, so it might not be the version that everyone can buy. The problem is the intaller, not CW. I have other versions installed, so my work around was to copy the entire directory from a vista machine and put it in Win 7.

 

Tim

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,031件の閲覧回数
J2MEJediMaster
Specialist I

Are you using 64-bit Win 7? The tools have only been validated to work on 32-bit Win 7 and Vista.

 

---Tom

 

0 件の賞賛
返信
2,031件の閲覧回数
TimMilliken
Contributor II

No, it is 32bit OS.

 

Tim

0 件の賞賛
返信
2,032件の閲覧回数
TimMilliken
Contributor II

Also it a version of Win 7 from an MSDN subcription, so it might not be the version that everyone can buy. The problem is the intaller, not CW. I have other versions installed, so my work around was to copy the entire directory from a vista machine and put it in Win 7.

 

Tim

0 件の賞賛
返信