CW 9.2 with MPC5121 - debug assembler view

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 9.2 with MPC5121 - debug assembler view

ソリューションへジャンプ
2,533件の閲覧回数
martinw
Contributor III

Hi,

 

Codewarrier Pro 9.2 with PowerPC MPC5121

 

Can anyone tell me if it's possible to single step through assembler code shown in the 'memory view'?

 

It something I'm used to in our Coldfire tools (Crossware) - once you are debugging some high level source, Crossware allows an assembly view to be opened, and a single step command then steps through the assembly level statements if that window has focus.

 

Thanks

 

Martin Wakely

Message Edited by martinw on 2009-06-26 02:05 PM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,562件の閲覧回数
CrasyCat
Specialist III

Hello

 

If you want to be able to step into assembly code:

  - Change format of Source pane in the Thread window from "Source" to "Mixed". This can be changed in the "Source List" edit box on the bottom of the thread view (next to the display of line & column number"

   - Now if you hit the step button you will step one assembly instruction at a time.

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,563件の閲覧回数
CrasyCat
Specialist III

Hello

 

If you want to be able to step into assembly code:

  - Change format of Source pane in the Thread window from "Source" to "Mixed". This can be changed in the "Source List" edit box on the bottom of the thread view (next to the display of line & column number"

   - Now if you hit the step button you will step one assembly instruction at a time.

 

CrasyCat

0 件の賞賛
返信
1,562件の閲覧回数
martinw
Contributor III
Many thanks, that's not easy to spot!
0 件の賞賛
返信