CW 7.2 Release Notes available separately?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 7.2 Release Notes available separately?

ソリューションへジャンプ
3,610件の閲覧回数
jbezem
Contributor III

I looked around the site for the release notes on CW 7.2 for Coldfire, available for download, to make a decision on when to upgrade our 7.1.2 installations.

However, I couldn't find them separately from the installation package, and I do not want to install the full package just yet, without knowing what's been done.

Can anyone point me to those release notes, or make them available in the forum?

 

Thanks,

 

Johan

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,180件の閲覧回数
vier_kuifjes
Senior Contributor I

Here you go (see attachments)...

 

Be warned though... if your app is Coldfire Lite based, it won't work when compiled with CW7.2.

CW7.2 uses the CPU registers to pass parameters to functions, whereas CW7.1.x used "regular" passing via the stack. Coldfire lite uses some assembly language routines that assume passing parameters via the stack. I managed to fix these routines and got Coldfire Lite running again, but there are still crucial things that don't work as supposed. For me it's a no-go.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,180件の閲覧回数
jbezem
Contributor III

Thanks for all three documents, very instructive, and foreboding a lot of unplanned work...

 

Regards,

 

Johan

0 件の賞賛
返信
2,180件の閲覧回数
vier_kuifjes
Senior Contributor I
This is probably a very important document... (see att)
0 件の賞賛
返信
2,181件の閲覧回数
vier_kuifjes
Senior Contributor I

Here you go (see attachments)...

 

Be warned though... if your app is Coldfire Lite based, it won't work when compiled with CW7.2.

CW7.2 uses the CPU registers to pass parameters to functions, whereas CW7.1.x used "regular" passing via the stack. Coldfire lite uses some assembly language routines that assume passing parameters via the stack. I managed to fix these routines and got Coldfire Lite running again, but there are still crucial things that don't work as supposed. For me it's a no-go.

0 件の賞賛
返信