Hello,
I recently upgraded my PC from Windows Vista to Windows 7 Home Premium (32bit). Under Vista, I had CodeWarrior MPC55xx v.2.4 running just fine. After installing Windows 7 and after restarting a few times, I tried running CodeWarrior 2.4, however every time I started the program it crashed. I assumed that some part of CodeWarrior was affected by the install, so I uninstalled it. I then downloaded CodeWarrior MPC55xx v.2.5 SE from the Freescale web site and attempted to install it. The installer extracted the installation files but as soon as it tried to perform the install it reported that the host OS is incompatible. The error message box had an "OK"/"Cancel" option, regardless of which I chose, that window closed and went back to the installation window with the "Next>" and "Cancel" options. Clicking the "Next>" caused the error window to pop up again, while "Cancel" ended the install. I retried the install with v.2.5 and also v.2.4, however the installer behaved exactly as I described above.
Is CodeWarrior MPC55xx v.2.x compatible with Windows 7 (32bit)? Are there any settings that must be made to ensure the installer and IDE run under Windows 7?
Thank you,
Dan
Hi Tom,
Thank you for the reply. I will try to work around this issue for now, however, our company will be upgrading to Windows 7 by the end of the year. Do you have any information about future compatibility with Windows 7?
Thank you, Dan
Sorry, but according to the CodeWarrior MPC55xx product summary page, only Vista is supported at this time.
---Tom