CF Flasher Query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CF Flasher Query

4,717 Views
TTA
Contributor I
Hi,

I am able to use CF Flasher to program the internal / external flash on the evaluation board M5282EVB ,

Will i be able to use CF flasher to program the MCF5282 internal flash, on a custom development board?

Also, are there any other BDM tools that can be used with the PE BDM cable to program the internal / external flash?

TTA
Labels (1)
0 Kudos
Reply
3 Replies

2,227 Views
fire
Contributor I
Thats right.I programed internal flash using CFFLASHER.
0 Kudos
Reply

2,227 Views
avm_ace
Contributor I

Hi,

 

I am using a MCF5329-powered custom board with a 32MB Intel P30 flash device. Can I program the flash using CFFlasher? If yes, please tell me as to how to go ahead with it.

 

Thanksand regards,

avm_ace

0 Kudos
Reply

2,227 Views
UK_CF_FAE
NXP Employee
NXP Employee

Hi TTA,

The good news is that CFFlasher _IS_ able to program the internal flash on your own target board based on MCF5282.

CFFlasher is a utlity written by Freescale in Austin, and published "as is" to the external web. CFF has a configuration system, so that you should be able to set up any internal/external flash for programming.

CodeWarrior for ColdFire V6.3 ships with a flash programming tool integrated into the IDE. Other, Third Party companies have flash programming utilities for ColdFire as well.

 

Mark

0 Kudos
Reply