Are there ANY SRIO CW Qonverge (B4860 preferred) projects?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Are there ANY SRIO CW Qonverge (B4860 preferred) projects?

1,742 次查看
markdouglas
NXP Employee
NXP Employee

Are there ANY SRIO CW Qonverge (B4860 preferred) projects?

or QorIQ?

 

we are just looking for a "raw" downloadable CW PA10.x project that can exercise SRIO

local loop-back and such

 

Thanks,

Mark

标签 (1)
0 项奖励
回复
3 回复数

1,498 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please download and install Netcomm 4.6 from NetComm Software Resources Product Summary Page, you will find SRIO driver in GA_4.6\NetCommSw\Peripherals, you could refer to C:\Program Files\Freescale\NetComm_Software\GA_4.6\NetCommSw\build\bare_p4080_cw_build\UseCases\controller\SRIO to deploy the project fro B4860.

Please also import NetCommSw and UserEnv projects into your workspace.

NetComm use Power ELF as the default compiler, please install Power ELF compiler in CodeWarrior 10.3 as the following.

Please open Help->Install New Software->Available Software Sites and check "FSL PA Build Tools", from "Work with" drop-down list select "http://freescale.com/lgfiles/updates/Eclipse/PA10_3/com.freescale.pa.buildtools_win", then choose "PA GCC ELF Build Tools Service Packs", then click "Next", CodeWarrior will perform online update automatically.

0 项奖励
回复

1,498 次查看
garryg
Contributor I

HI Yiping,

Has anyone tried this project on the B4860 or T4240 devices yet?

Do we know if it will work?

Thanks,

Garry

0 项奖励
回复

1,498 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Garry,

NetComm 4.6 should be tested before released.

Thanks,

Yiping

0 项奖励
回复