36-bit memory assignment in Codewarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

36-bit memory assignment in Codewarrior

7,280件の閲覧回数
敏赵
Contributor I

Hi

We designed a target board using p2020 CPU referring to the design of P2020RDB-PC. I must use 36-bit memory map in my target board.

Before I flash uboot to my target board, I tried to flash official 36bit-uboot to the P2020RDB-PC.

I modify relevant memory addresses in P2020RDB-PC_init_sram_flash.tcl, as following:

 

mem [CCSR 0xc08] = 0x00Fff000

mem [CCSR 0xca8] = 0x00Ff8000

mem [CCSR 0x0] = 0x00Fe0000

reg ${CAM_GROUP}L2MMU_CAM1  = 0x500003CAFC08000FE000000FE0000001

reg ${CAM_GROUP}L2MMU_CAM2  = 0x70000FCAFC08000FFF00000FFF000001

reg ${CAM_GROUP}L2MMU_CAM7  = 0x500003CAFC08000FF800000FF8000001

reg ${SPR_GROUP}HID0 = 0x00004080

reg ${SPR_GROUP}MAS7 = 0x0000000F 

 

When I debug the initialization file, the console information is as followed:

12670_12670.jpgQQ图片20140621105355.jpg

12677_12677.jpgQQ图片20140621105913.jpg

 

What mistakes have I made in my .tcl file?

Thanks a lot

 

Best regards,

Min Zhao

Original Attachment has been moved to: P2020RDB-PC_init_sram_flash.tcl.txt.zip

ラベル(1)
0 件の賞賛
返信
14 返答(返信)

6,519件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

First I think you could use P2020RDB-PC_init_sram_flash.tcl to initialize your customize target board and flash u-boot.(Probably you only need to modify the address for NOR Flash)

In you want to modify the initialization file to coincide with the 36bit address space, please pay attention to the following.

1. MMU TLB configuration, please note effective addresses are 32 bit, please refer to the table "e500v2 TLB1 Registers" in CW_PA_v10.3.3\PA\Help\PDF\Targeting_PA_Processors.pdf.

    # MMU  initialization

    # define 256KB  TLB1 entry 3: 0x00000000 - 0x0003FFFF; for internal chip SRAM

    reg ${CAM_GROUP}L2MMU_CAM3  = 0x400001C0FC0800000000000000000001

    # define 1MB    TLB1 entry 1: 0xE0000000 - 0xE00FFFFF; for CCSR Space, non cacheable

    reg ${CAM_GROUP}L2MMU_CAM1  = 0x500003CAFC080000E0000000E0000001

    # define 16MB  TLB1 entry 2: 0xFFF000000 - 0xFFFFFFFF; for Local Bus, cache inhibited

    reg ${CAM_GROUP}L2MMU_CAM2  = 0x70000FCAFC08000FFF000000FF000001

    # define 1MB    TLB1 entry 7: 0xFF8000000 - 0xF80FFFFF; for NAND, cache inhibited

    reg ${CAM_GROUP}L2MMU_CAM7  = 0x500003CAFC08000FF8000000F8000001

2. For CCSRBAR, please configure as the default

mem [CCSR 0x0] = 0x000e0000

set CCSRBAR 0xe0000000

Your configuration is correct, but if specifying variable CCSRBAR as 0xfe0000000, there is some problem in the tcl script to compute the value more than 32bit.

Attached an initialization file I modified based on yours.


Have a great day,
Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,519件の閲覧回数
敏赵
Contributor I

I have flash 36bit-uboot to the custom p2020rdb-pc successfully by the tcl you gave to me.

Then I modified the tcl to math with my target board.But when I modified theR L2SRBAEA0

mem [CCSR 0x20104] = x00000000--------->0x0000000f

It failed to flash the uboot.

Then I use the mem [CCSR 0x20104] = 0x00000000, it worked.

Did that mean I should set the L2SRBAEA0 at 0x00000000?


And as you suggested, I need to modify NOR/NAND BR registers with 36bit physical addresses?

How should I modify NOR/NAND BR registers? what should I refer to NOR/NAND BR registers

Thanks a lot.

Best regards,

Min Zhao

0 件の賞賛
返信

6,519件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

[CCSR 0x20104] should be 0x00000000, the physical address of SRAM is 0_00000000 and effective address is 00000000, in this initialization file DDR SDRAM is not considered about, and L2 to SRAM is the replacement of DDR, please refer to MMU  TLB1 entry 3 is also configured like this.

About BA of BR register configuration, I think I made a mistake, it should be the upper 17bits of 32 bit address.

pastedImage_0.png

For details,please refer to eLBC_BRn and ORn in P2020RM.

The following is u-boot code, you could have a reference.

#define CONFIG_SYS_FLASH_BASE      0xef000000

#ifdef CONFIG_PHYS_64BIT

#define CONFIG_SYS_FLASH_BASE_PHYS  0xfef000000ull

#else

#define CONFIG_SYS_FLASH_BASE_PHYS CONFIG_SYS_FLASH_BASE

#endif

#define CONFIG_FLASH_BR_PRELIM (BR_PHYS_ADDR(CONFIG_SYS_FLASH_BASE_PHYS) | BR_PS_16 | BR_V)

#define CONFIG_FLASH_OR_PRELIM      0xff000ff7

#define BR_PHYS_ADDR(x) ((u32)(x) & 0xffff8000)


Have a great day,
Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,519件の閲覧回数
敏赵
Contributor I

On the base of my 4G DDR, need I modify the following addresses in u-boot code:

#define CONFIG_SYS_INIT_L2_ADD0xf8f80000
#define CONFIG_SYS_TEXT_BASE0xf8f82000
#define CONFIG_SYS_TEXT_BASE0xeff80000
#define CONFIG_RESET_VECTOR_ADDRESS0xeffffffc
#define CONFIG_SYS_CCSRBAR0xffe00000

They didn't have the judgment statement:  #ifdef CONFIG_PHYS_64BIT

Best regards,

Min Zhao

0 件の賞賛
返信

6,519件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Min Zhao,

I don't think you need to modify these addresses in u-boot, please refer to the following memory map for P2020RDB 36 bit physical addresses allocation in u-boot, probably you need to modify the Flash base address according to your target.

Start Physical Address

End Physical Address

Definition

Size

0x000000000

0xbffffffff

DDR

48G

0xc20000000

0xc3fffffff

PCI Express 2 MEM

512MB

0xc00000000

0xc1fffffff

PCI Express 1 MEM

512MB

0xfef000000

0xfefffffff

FLASH

16M

0xfffc00000

0xfffc3ffff

PCI IO range

256K

0xfff800000

0xfff8fffff

NAND

1M

0xfffe00000

0xfffefffff

CCSR

1M

0xfffa00000

0xfffafffff

CPLD

1M

0xfffb00000

0xfffb7ffff

vsc7385 switch

1M

0xfffd00000

0xfffd03fff

L1 for stack

16K

0xffff00000

0xffff7ffff

L2 SDRAM

512K


Have a great day,
Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,519件の閲覧回数
敏赵
Contributor I

I tried to modify the address of L2 to 0xf_f8f80000 and the base address of CCSR to 0xf_ffe00000. But when I make it, there is an error in making start.o


#define CONFIG_SYS_INIT_L2_ADDR0xff8f80000
#define CONFIG_SYS_CCSRBAR  0xfffe00000

How can I modify the base address of L2 and CCSR?

Best regards,

Min Zhao

0 件の賞賛
返信

6,519件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

In 36 bit u-boot, CCSRBAR has already been defined at 0xf_ffe00000.

Please pay attention to the following definition in include/mpc85xx.h.

#ifndef CONFIG_SYS_CCSRBAR_PHYS_HIGH

#ifdef CONFIG_PHYS_64BIT

#define CONFIG_SYS_CCSRBAR_PHYS_HIGH    0xf

#else

#define CONFIG_SYS_CCSRBAR_PHYS_HIGH    0

#endif

CONFIG_SYS_TEXT_BASE and CONFIG_RESET_VECTOR_ADDRESS are 32 bit effective addresses, please don't touch them.


Have a great day,
Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,519件の閲覧回数
敏赵
Contributor I

We have replaced our 4G DDR to the official 1G DDR chip, and we successfully boot the board.

Did it mean I only need modify the configurations of DDR in u-boot matching to our 4G DDR on the base of above? What's more I don't need to modify anything else codes as long as I make 36-bit u-boot?

Best regards,

Min Zhao

0 件の賞賛
返信

6,519件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Min Zhao,

Please pay attention to LAW size configuration and TLB configuration.

In the file include/configs/p1_p2_rdb_pc.h

#define CONFIG_SYS_SDRAM_SIZE_LAW LAW_SIZE_1G

In the file board/freescale/p1_p2_rdb_pc/tlb.c

SET_TLB_ENTRY(1, CONFIG_SYS_DDR_SDRAM_BASE, CONFIG_SYS_DDR_SDRAM_BASE,
MAS3_SX|MAS3_SW|MAS3_SR, 0,
0, 8, BOOKE_PAGESZ_1G, 1),

Please note, the effective address is 32 bit, total 4 G memory space.


Have a great day,
Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,519件の閲覧回数
敏赵
Contributor I

I have modify the codes as following:

#define CONFIG_SYS_SDRAM_SIZE_LAW LAW_SIZE_4G


SET_TLB_ENTRY(1, CONFIG_SYS_DDR_SDRAM_BASE, CONFIG_SYS_DDR_SDRAM_BASE,

  MAS3_SX|MAS3_SW|MAS3_SR, 0,

  0, 8, BOOKE_PAGESZ_2G, 1),

  SET_TLB_ENTRY(1, CONFIG_SYS_DDR_SDRAM_BASE + 0x40000000,

  CONFIG_SYS_DDR_SDRAM_BASE + 0x40000000,

  MAS3_SX|MAS3_SW|MAS3_SR, MAS2_I|MAS2_G,

  0, 9, BOOKE_PAGESZ_2G, 1),

But it still showed 2GB umapped.

Do I need to modify more configurations?

Best regards,

Min Zhao

0 件の賞賛
返信

6,519件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

I think it is fine to map 2G DDR memory, because total 4G effective memory space, and it is needed to leave another 2G for other devices. It is necessary to leave part of DDR memory unmapped.

Please refer to "Memory map" section in include/configs/p1_p2_rdb_pc.h.

Please make sure DDR memory allocation is not overlapped with other devices.


Have a great day,
Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,519件の閲覧回数
敏赵
Contributor I

My memory map is DDR  0x00000000 ~ 0xffffffff, other's all use the default 36-bit.

There is only L2's base address must be 32-bit(0xf8f80000).

Is this the reason of it?

Best regards,

Min Zhao

0 件の賞賛
返信

6,519件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Now we talk about effective addresses(32bit), please don't make it confused with physical addresses(36bit).

The following is the memory map of effective address, and for the physical addresses, please refer to the above table I pasted previously.

/*

* Memory map

*

* 0x0000_0000 0x7fff_ffff      DDR            Up to 2GB cacheable

* 0x8000_0000 0xdfff_ffff      PCI Express Mem 1.5G non-cacheable(PCIe * 3)

* 0xec00_0000 0xefff_ffff      NOR flash      Up to 64M non-cacheable CS0/1

* 0xf8f8_0000 0xf8ff_ffff      L2 SRAM        Up to 512K cacheable

*  (early boot only)

* 0xff80_0000 0xff80_7fff      NAND flash      32K non-cacheable      CS1/0

* 0xff98_0000 0xff98_ffff      PMC            64K non-cacheable      CS2

* 0xffa0_0000 0xffaf_ffff      CPLD            1M non-cacheable        CS3

* 0xffb0_0000 0xffbf_ffff      VSC7385 switch  1M non-cacheable        CS2

* 0xffc0_0000 0xffc3_ffff      PCI IO range    256k non-cacheable

* 0xffd0_0000 0xffd0_3fff      L1 for stack    16K cacheable

* 0xffe0_0000 0xffef_ffff      CCSR            1M non-cacheable

*/

If needed, please read "Memory Management Units" in e500 core reference manual(E500CORERM.pdf).


Have a great day,
Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------


Have a great day,
Yiping Wang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,519件の閲覧回数
敏赵
Contributor I

I'm a little confused. Do you mean the effective address of DDR is only up to 2G, and the effective address is translated to 4G by tlb1?

Then how should I set CONFIG_SYS_SDRAM_SIZE_LAW LAW_SIZE? and did I successfully modify the code in tlb.c?

Best regards,

Min Zhao

0 件の賞賛
返信