why my codewarrior HCS08 5.1 create a new project will close the codewarrior window?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why my codewarrior HCS08 5.1 create a new project will close the codewarrior window?

Jump to solution
2,547 Views
KingZhang
Contributor I
why my codewarrior HCS08 5.1  create a new project or click open project button ,will close the codewarrior window?but no this problem on my notebook .
 
I think the codewarrior if ready to using "open folder" or "create file or folder" window ,this problem will appear.
 
my computer operating system is Windows XP SP2.
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,556 Views
CompilerGuru
NXP Employee
NXP Employee
High KingZhang,

there has been a reported incompatibility with MS Office 2007 with these symptoms in this forum.
See this thread for the case, it also contains a workaround.

http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=3747&query.id=4082#M3...


Daniel

View solution in original post

0 Kudos
Reply
2 Replies
1,557 Views
CompilerGuru
NXP Employee
NXP Employee
High KingZhang,

there has been a reported incompatibility with MS Office 2007 with these symptoms in this forum.
See this thread for the case, it also contains a workaround.

http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=3747&query.id=4082#M3...


Daniel
0 Kudos
Reply
1,556 Views
KingZhang
Contributor I
Hi,CompilerGuru
 
I'm Uncheck "Run this program in compatibility mode for". it works beautifully.
 
Thanks your help,
 

 
0 Kudos
Reply