the CW10.6 command line tools question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the CW10.6 command line tools question

ソリューションへジャンプ
1,793件の閲覧回数
wangpeng
Contributor I

Hi:

I link a project used the command line tools ,and  the commands is copy from CW10.6 setting ,but the tools had an err "undefined: '__start'",when i run the command .I can find the file"__start.c",but I do not know how to define the __start?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,637件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello peng

Please check the settings for the access path has been configured correctly, it should contains the path for the head file which includes the external function declaration for '__start '.

For details, please refer to the compiler manual for your MCU.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,638件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello peng

Please check the settings for the access path has been configured correctly, it should contains the path for the head file which includes the external function declaration for '__start '.

For details, please refer to the compiler manual for your MCU.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,637件の閲覧回数
wangpeng
Contributor I

Hi:

I had check the settings, and add the path of the "__start.c",and the header files , but it had a Undefine "__start" err also.and can you provide some examples about the command line tools for mpc56xx to me? or the example about CW API .

i can found several datasgeet about the commandline tools.

thank you!

2016-05-06

王鹏

控制部

北京亿华通科技股份有限公司

地址:北京市海淀区永丰产业基地永澄北路绿海大厦A座4层

邮编:100094

电话:+86 10 56382035/36/37/38-120

传真:+86 10 56382035-162

手机:13167398738

网址:http://www.sinohytec.com

邮箱:[email protected]

发件人:TICS_Fiona <[email protected]>

发送时间:2016-05-04 15:34

主题:Re: - the CW10.6 command line tools question

收件人:"peng wang"<[email protected]>

抄送:

NXP Community

the CW10.6 command line tools question

reply from Xin Kuang in CodeWarrior for MCU - View the full discussion

Hello peng

Please check the settings for the access path has been configured correctly, it should contains the path for the head file which includes the external function declaration for '__start '.

For details, please refer to the compiler manual for your MCU.

Best Regards

Fiona Kuang

TIC - Technical Information Center

0 件の賞賛
返信