adc in MC56F84789

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

adc in MC56F84789

2,129 次查看
josephxavier
Contributor III

can any share simple ADC code for MC56F84789 with details

标签 (1)
0 项奖励
回复
3 回复数

1,813 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello joseph

56F84789 has two ADC modules: 16bit SAR ADC and 12bit Cyclic ADC.

The attached example is a project for SAR ADC which is working in hardware triggering mode.

 

In addition, user can download the example projects for 56F84789 from:

http://www.nxp.com/products/microcontrollers-and-processors/more-processors/dsp-dsc/dscs/mc56f84xxx/...

The example package is under ‘Software Development Tools -> Lab and Test Software’ in the above page.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,813 次查看
josephxavier
Contributor III

thanks for the sample project , it will  a great help  if u could suggest a document(specific application note or something) to under stand the adc functionality in  mc56f84789 properly

0 项奖励
回复

1,813 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello joseph

For details of ADC functionality, please refer to the reference manual:

http://cache.nxp.com/files/dsp/doc/ref_manual/MC56F847XXRM.pdf

For the ADC conjunction with other modules, you may refer to:

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4583.pdf

Hope this helps!

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------