register allocation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,427件の閲覧回数
stefanodimasci1
Contributor III

Hello,

 

I need to be sure that a register won't be used during register allocation in GCC because I need it for some assembly level checks. Does anybody know what kind of directive I have to put in codewarrior?

 

 

Thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,323件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Stefano,

You're using CW for MCU v10.6 for MPC56XX.

Now If I understand correctly you request, you want to reserve a register.

I've found a note  explaining how to do that in the \CW MCU v10.6.4\MCU\Help\PDF\MCU_Power-Architecture_Compiler.pdf manual.

Please have a look pages 258 - 261

     14.2 Additional Small Data Sections

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,323件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Stefano,

Can you please let me know what is the development tool chain you're using and the Processor ?

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,323件の閲覧回数
stefanodimasci1
Contributor III

I'm using the deafult GNU toolchain on codewarrior for the MPC5643L.

0 件の賞賛
返信
2,324件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Stefano,

You're using CW for MCU v10.6 for MPC56XX.

Now If I understand correctly you request, you want to reserve a register.

I've found a note  explaining how to do that in the \CW MCU v10.6.4\MCU\Help\PDF\MCU_Power-Architecture_Compiler.pdf manual.

Please have a look pages 258 - 261

     14.2 Additional Small Data Sections

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信