Hello, and welcome to the forum.
The suitability and approach to using the RTI (or maybe MTIM) for generating a 3.24 second delay will depend on the timing accuracy that you require, and the crystal frequency you are using. Some crystal frequencies will be more convenient than others, and potentially produce greater accuracy.
For example, if you were using a 32.768 kHz watch crystal as the external reference, your required timing period would be represented by 106168 clock cycles. This has factors of 8 x 23 x 577. The last factor exceeds an 8-bit modulo count.
With this example, the approach might be to set the RTI modulo value to 184 (8 x 23), with a prescale value of 1. This would generate an interrupt every 5.62 milliseconds. Within the ISR code, you might decrement a global variable that starts with an initial value of 577. When the variable decrements to zero, the required delay period would have elapsed. Make sure that you clear the RTI flag within the ISR code.
With a selected higher frequency crystal, you might be able to make use of the prescaler, and possibly achieve the delay period with a single interrupt, i.e. with a prescaled clock of 50Hz, and a modulo value of 162, or maybe a prescaled clock of 75Hz, and a modulo value of 243. Of course, the crystal frequency will also need to be suitable for the external reference range needed by the ICS module. With this approach, crystal frequencies of 5.000 MHz or 4.9152 MHz would appear suitable.
For future reference, threads concerning the operation of the HCS08 MCU hardware would usually be posted in the 8-bit forum.
Regards,
Mac