Does CW special or basic edition support Kinetis and MQX?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does CW special or basic edition support Kinetis and MQX?

Jump to solution
1,582 Views
ayang
Contributor I

I am new to Kinetis and MQX and would like to evalute them. Does CW special edition (128KB limit to Kinetis) or basic edition (512KB limit to Kinetis) support Kinetis and MQX?

Labels (1)
0 Kudos
Reply
1 Solution
1,413 Views
J2MEJediMaster
Specialist I

As you probably suspect, the Special and Stanard Editions might not have sufficient capabilities (in terms of code size limits or other restrictions) to work with the MQX RTOS. If you are going to evaluate the software, you might as well download the fully-featured Evaluation version of CodeWarrior and try it for 30 days to accurately assess the capabilities of the product, rather than trip over the limitations.

 

The short answer to your question is that the Special Edition and Standard Edition do support the Kinetis part.

 

---Tom

View solution in original post

0 Kudos
Reply
1 Reply
1,414 Views
J2MEJediMaster
Specialist I

As you probably suspect, the Special and Stanard Editions might not have sufficient capabilities (in terms of code size limits or other restrictions) to work with the MQX RTOS. If you are going to evaluate the software, you might as well download the fully-featured Evaluation version of CodeWarrior and try it for 30 days to accurately assess the capabilities of the product, rather than trip over the limitations.

 

The short answer to your question is that the Special Edition and Standard Edition do support the Kinetis part.

 

---Tom

0 Kudos
Reply