program data Flash using DSC Flash Programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

program data Flash using DSC Flash Programmer

3,866 Views
HardyCao
Contributor I

Hi all,

Recently, I try to use Multilink Universal to download the data to the Data Flash of MC56F8345, I met below program even I used the same file which just generated by dumping Flash by DSC Flash programmer. 

 

fl::target -lc "MC56F8345_FLASH_LDM_PnE U-MultiLink"
fl::target -b 0x2fc00 0x400
fl::target -v off -l off
cmdwin::fl::device -d "MC56F8345_X_FLASH" -o "4kx16x1" -a 0x1000 0x1fff
cmdwin::fl::image -f "C:\\Users\\HardyCao\\Desktop\\SBD\\Project\\SAM\\Software\\firmware\\ATM--3355.BIN" -t "Binary/Raw Format" -re off -oe off
cmdwin::fl::erase image
Beginning Operation ...
-------------------------
Nothing to erase. No sectors selected
Performing target initialization ...
Erase Command Succeeded.
cmdwin::fl::write
-------------------------
Flash Operation. ...
Programming ...
Programming warning. Can't program 8192 bytes to address 0x0 because this range isn't included in the selected modules!
Program Command Succeeded
Flash Operation. done
cmdwin::fl::image -f "C:\\Users\\HardyCao\\Desktop\\SBD\\Project\\SAM\\Software\\firmware\\ATM-3355.BIN" -t "Auto Detect" -re off -oe off
cmdwin::fl::verify
-------------------------
C:\Users\HardyCao\Desktop\SBD\Project\SAM\Software\firmware\ATM-3355.BIN
Flash Operation. ...
Auto-detection is successful.
File is of type Binary/Raw Format.

Programming warning. Can't verify 8192 bytes to address 0x0 because this range isn't included in the selected modules!
Verify Command Succeeded

0 Kudos
Reply
1 Reply

3,721 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you use multilink Universal device to download code to MC56F8345 flash, I suppose that that you can use third party PROGDSC tools from the link, the tools is free of charge.

https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320181&productTab=5

 

If your PC uses Win10 OS, I suppose that you can install the CodeWarrior for MCU ver11.x, and use the tools to download S-Record file to flash of MC56F8345.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply