problems with CW05

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,811件の閲覧回数
teruko
Contributor I
Hello,
I'd like to use the project EVK_Switch_Demo (this project is  included in BeeKit Wireless Connectivity Toolkit Rev. 0.0 - 10/2006)  with CW v5.0 for HC(s)08, but when I link, I have the follow message:
Link Error : L1936: ELF output: Burner Error: Could not open the Link
Burner output file.

Link Error : Link failed
Please, what can I do to run this ready project ( there is a  message that this project was created with CW v3.1)??
Thank you!!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,911件の閲覧回数
trytohelp
NXP Employee
NXP Employee
This problem has been logged in the Freescale data base under the 1-342881601.
This issue will be investiagte by the support team.
 
Pascal

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,912件の閲覧回数
trytohelp
NXP Employee
NXP Employee
This problem has been logged in the Freescale data base under the 1-342881601.
This issue will be investiagte by the support team.
 
Pascal
0 件の賞賛
返信