problems with CW05

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problems with CW05

Jump to solution
2,879 Views
teruko
Contributor I
Hello,
I'd like to use the project EVK_Switch_Demo (this project is  included in BeeKit Wireless Connectivity Toolkit Rev. 0.0 - 10/2006)  with CW v5.0 for HC(s)08, but when I link, I have the follow message:
Link Error : L1936: ELF output: Burner Error: Could not open the Link
Burner output file.

Link Error : Link failed
Please, what can I do to run this ready project ( there is a  message that this project was created with CW v3.1)??
Thank you!!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,979 Views
trytohelp
NXP Employee
NXP Employee
This problem has been logged in the Freescale data base under the 1-342881601.
This issue will be investiagte by the support team.
 
Pascal

View solution in original post

0 Kudos
Reply
1 Reply
1,980 Views
trytohelp
NXP Employee
NXP Employee
This problem has been logged in the Freescale data base under the 1-342881601.
This issue will be investiagte by the support team.
 
Pascal
0 Kudos
Reply