problem with windrvr6.inf !!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

problem with windrvr6.inf !!

跳至解决方案
6,120 次查看
Edward_Kang
Contributor I
When installing the CW12_V4_6.exe, which is the CodeWarrior Development Studio for HCS12X Microcontrollers, the setup cannot be finished because of the following problem.
 
Failed to install the INF file(C:\Windows\inf\windrvr6.inf)
Eroor updating the driver(hwid:*WINDRVR6) with the INF file : cannot find the designated file.
 
 
I use Windows Vista Home Premium and I want to know the solution.
(I already did format and setup again to solve the problem, but ..)


Message Edited by Edward.Kang on 2007-09-04 06:56 AM
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,754 次查看
CrasyCat
Specialist III
Hello
 
CodeWarrior for HCS12 V4.6 does not support Windows Vista.
The future CodeWarrior for HC(S)12(X) V5.0 will support Windows Vista.
This release is planned for end of this year.
 
You may want to look at the following thread
 
Some people could install CodeWarrior HCS12 on Vista and provide some hints.
Note that Freescale did not validate the tools on Vista and we will not provide support for Vista specific issues when running V4.6.
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,755 次查看
CrasyCat
Specialist III
Hello
 
CodeWarrior for HCS12 V4.6 does not support Windows Vista.
The future CodeWarrior for HC(S)12(X) V5.0 will support Windows Vista.
This release is planned for end of this year.
 
You may want to look at the following thread
 
Some people could install CodeWarrior HCS12 on Vista and provide some hints.
Note that Freescale did not validate the tools on Vista and we will not provide support for Vista specific issues when running V4.6.
 
CrasyCat
0 项奖励
回复