osek part number description

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

osek part number description

ソリューションへジャンプ
2,622件の閲覧回数
hotashu
Contributor III

I am intresting in osek. i find this link:</p>

 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=OSEKTURBO&tab=Buy_Parametric_Tab&from...

but there is no description about the part number list.
for example:
CWX-OSK-D100K-DL
CWX-OSK-D10K-DL
CWX-OSK-D1K-DL
CWX-OSK-D200-DL
CWX-OSK-D200K-DL
CWX-OSK-D2MIL-DL
CWX-OSK-D500K-DL
CWX-OSK-UNLTD-DL


the price is different for each of them.
it is very appreciated if anybody can tell me the different.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,428件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

hi Hotas,

when click the icon "i" follows each partnumber, you will see the description for the partnumber.

for example,

the description for CWX-OSK-D10K-DL is 'OSEK DISTRIBUTION LICENSE FOR <10K UNITS'

for CWX-OSK-D1K-DL, it means "OSEK DISTRIBUTION LICENSE FOR <1K UNITS"

the main difference is in the distribution number.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,429件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

hi Hotas,

when click the icon "i" follows each partnumber, you will see the description for the partnumber.

for example,

the description for CWX-OSK-D10K-DL is 'OSEK DISTRIBUTION LICENSE FOR <10K UNITS'

for CWX-OSK-D1K-DL, it means "OSEK DISTRIBUTION LICENSE FOR <1K UNITS"

the main difference is in the distribution number.

0 件の賞賛
返信
2,428件の閲覧回数
hotashu
Contributor III

any news?

0 件の賞賛
返信
2,428件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

I've re-sent an email this morning.

It seems colleagues working for Osek are in vacation.

Very sorry for the delay.

I will keep you informed.

Pascal

0 件の賞賛
返信
2,428件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Hotas,

Thanks for the question.

I've contacted colleague.

We will keep you informed.

Regards

Pascal

0 件の賞賛
返信