osek part number description

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

osek part number description

Jump to solution
2,565 Views
hotashu
Contributor III

I am intresting in osek. i find this link:</p>

 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=OSEKTURBO&tab=Buy_Parametric_Tab&from...

but there is no description about the part number list.
for example:
CWX-OSK-D100K-DL
CWX-OSK-D10K-DL
CWX-OSK-D1K-DL
CWX-OSK-D200-DL
CWX-OSK-D200K-DL
CWX-OSK-D2MIL-DL
CWX-OSK-D500K-DL
CWX-OSK-UNLTD-DL


the price is different for each of them.
it is very appreciated if anybody can tell me the different.

Labels (1)
0 Kudos
Reply
1 Solution
2,371 Views
Rick_Li
NXP Employee
NXP Employee

hi Hotas,

when click the icon "i" follows each partnumber, you will see the description for the partnumber.

for example,

the description for CWX-OSK-D10K-DL is 'OSEK DISTRIBUTION LICENSE FOR <10K UNITS'

for CWX-OSK-D1K-DL, it means "OSEK DISTRIBUTION LICENSE FOR <1K UNITS"

the main difference is in the distribution number.

View solution in original post

0 Kudos
Reply
4 Replies
2,372 Views
Rick_Li
NXP Employee
NXP Employee

hi Hotas,

when click the icon "i" follows each partnumber, you will see the description for the partnumber.

for example,

the description for CWX-OSK-D10K-DL is 'OSEK DISTRIBUTION LICENSE FOR <10K UNITS'

for CWX-OSK-D1K-DL, it means "OSEK DISTRIBUTION LICENSE FOR <1K UNITS"

the main difference is in the distribution number.

0 Kudos
Reply
2,371 Views
hotashu
Contributor III

any news?

0 Kudos
Reply
2,371 Views
trytohelp
NXP Employee
NXP Employee

Hi,

I've re-sent an email this morning.

It seems colleagues working for Osek are in vacation.

Very sorry for the delay.

I will keep you informed.

Pascal

0 Kudos
Reply
2,371 Views
trytohelp
NXP Employee
NXP Employee

Hi Hotas,

Thanks for the question.

I've contacted colleague.

We will keep you informed.

Regards

Pascal

0 Kudos
Reply