no connection after flash erase/program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

no connection after flash erase/program

Jump to solution
2,970 Views
electronicfan
Contributor II
hey all,

i have some trouble with my HCS08-Controller.
He works fine before i used my own flash earse/program function.
I got an illegal_BP and now i can't connect my controller.
SYNC stopped, TARGET-SELF-RESET,....

Do you have any idea?

electronicfan
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,985 Views
electronicfan
Contributor II
hey,
i use an open source programmer to programm an single controller.

Now i use a professional programmer from p&e and it works fine.
I think, their are a lot of software problems in the firmware of the open source programmer.

View solution in original post

0 Kudos
Reply
2 Replies
1,986 Views
electronicfan
Contributor II
hey,
i use an open source programmer to programm an single controller.

Now i use a professional programmer from p&e and it works fine.
I think, their are a lot of software problems in the firmware of the open source programmer.
0 Kudos
Reply
1,985 Views
Evgenij
Contributor III
Just a question - do you use single microcontroller or with evaluation board? And with what interface do you flash your controller (RS232 or BDM)?
0 Kudos
Reply