no connection after flash erase/program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

no connection after flash erase/program

ソリューションへジャンプ
2,948件の閲覧回数
electronicfan
Contributor II
hey all,

i have some trouble with my HCS08-Controller.
He works fine before i used my own flash earse/program function.
I got an illegal_BP and now i can't connect my controller.
SYNC stopped, TARGET-SELF-RESET,....

Do you have any idea?

electronicfan
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,963件の閲覧回数
electronicfan
Contributor II
hey,
i use an open source programmer to programm an single controller.

Now i use a professional programmer from p&e and it works fine.
I think, their are a lot of software problems in the firmware of the open source programmer.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,964件の閲覧回数
electronicfan
Contributor II
hey,
i use an open source programmer to programm an single controller.

Now i use a professional programmer from p&e and it works fine.
I think, their are a lot of software problems in the firmware of the open source programmer.
0 件の賞賛
返信
1,963件の閲覧回数
Evgenij
Contributor III
Just a question - do you use single microcontroller or with evaluation board? And with what interface do you flash your controller (RS232 or BDM)?
0 件の賞賛
返信