memory not recognised

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

memory not recognised

ソリューションへジャンプ
1,537件の閲覧回数
juliancox
Contributor V

I am using CW10 (CW11 gives the same problem) with a S08SH4. When this device could not provide sufficient memory for the project I changed the Target device to a S08SH8. I added this device using the ProcessorExpert Hardware option. I deleted all references to the SH4 devices in the Components window leaving only the  SH8 devices, but I get debugger errors showing that there is no flash memory available from 0xE000 to 0xEFFF and no RAM from 0x0180 to 0x027F. The memory configuration file (.mem) still shows the device as a SH4 with SH4 memory limits. The .prm file is correct for the SH8. I tried to edit the .mem file but it gave an error and would not debug. if I delete the .mem file the debugger says it cannot find the .mem file. What do I do?

タグ(1)
0 件の賞賛
返信
1 解決策
1,419件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Julian Cox  ,

How about change the Debug Configuration to MC9S08SH8 as below :

pastedImage_1.png

Also create a new project with S08SH8 , then use the  two debugger files "MC9S08SH8.mem" and "MC9S0BSH8"

instead of S08SH4 files .

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,420件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Julian Cox  ,

How about change the Debug Configuration to MC9S08SH8 as below :

pastedImage_1.png

Also create a new project with S08SH8 , then use the  two debugger files "MC9S08SH8.mem" and "MC9S0BSH8"

instead of S08SH4 files .

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------