librarian print format setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

librarian print format setting

2,588件の閲覧回数
katsumikimoto
Contributor I

I found settings of librarian, print format and scan format can not be saved.

I changed the setting 'int' to 'int_FP' and that worked.

But after I restarted CodeWarrior the setting are reset to 'int'.

I tried on CW 10.4 and 10.5 and got the same result.

Any idea or points to preserve changed setting of print and scan formats?

 

Thanks,

 

--Katsumi Kimoto

ラベル(1)
タグ(4)
0 件の賞賛
返信
4 返答(返信)

2,323件の閲覧回数
katsumikimoto
Contributor I

Sorry, I am using Kinetis K60 with floating point K60FN1M0.

--Katsumi

0 件の賞賛
返信

2,323件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

i couldn't reproduce your problem.

please try to remove .metadata folder in your current workapce then restart CW and test it again.

if the problem persists,

can you please send us your project so that we can test the problem on our side?

2,323件の閲覧回数
katsumikimoto
Contributor I

I tested on newly created, almost empty project from commander window

and it preserved my  settings of int_FP of print format.

I found the problem is not in  CodeWarrior, but in my project.

I use FNET TCP/IP 2.5.0 library which causes this problem in any way.

Sample project twrk60n512_shell  of FNET also did not preserve the settings.

I have checked the latest version of FNET,  2.6.2, and its demo project preserved

the settings.

I will upgrade FNET library in my project.

Thank you for your help.

Katsumi

0 件の賞賛
返信

2,323件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome!

0 件の賞賛
返信