librarian print format setting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

librarian print format setting

2,558 次查看
katsumikimoto
Contributor I

I found settings of librarian, print format and scan format can not be saved.

I changed the setting 'int' to 'int_FP' and that worked.

But after I restarted CodeWarrior the setting are reset to 'int'.

I tried on CW 10.4 and 10.5 and got the same result.

Any idea or points to preserve changed setting of print and scan formats?

 

Thanks,

 

--Katsumi Kimoto

标签 (1)
标记 (4)
0 项奖励
回复
4 回复数

2,293 次查看
katsumikimoto
Contributor I

Sorry, I am using Kinetis K60 with floating point K60FN1M0.

--Katsumi

0 项奖励
回复

2,293 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

i couldn't reproduce your problem.

please try to remove .metadata folder in your current workapce then restart CW and test it again.

if the problem persists,

can you please send us your project so that we can test the problem on our side?

2,293 次查看
katsumikimoto
Contributor I

I tested on newly created, almost empty project from commander window

and it preserved my  settings of int_FP of print format.

I found the problem is not in  CodeWarrior, but in my project.

I use FNET TCP/IP 2.5.0 library which causes this problem in any way.

Sample project twrk60n512_shell  of FNET also did not preserve the settings.

I have checked the latest version of FNET,  2.6.2, and its demo project preserved

the settings.

I will upgrade FNET library in my project.

Thank you for your help.

Katsumi

0 项奖励
回复

2,293 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome!

0 项奖励
回复