jungo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

jungo

8,071件の閲覧回数
richardtolleson
Contributor I

I am having trouble running 2 different versions of freescale software and keeping the jungo drivers working. I need to run cw_hc12_v5.1_special and cw_mcu_v10.1_se.

the 10.1 installs and runs perfect. v5.1 will install but it fails to load and run the jungo driver. it fails even if i am logged in as administrator, right click and "run as administrator",

virus scan is disabled, and it is removed from the domain.

I am running windows 7 enterprise.

ラベル(1)
タグ(1)
0 件の賞賛
返信
9 返答(返信)

7,884件の閲覧回数
kef2
Senior Contributor V

Richard, try installing CW5.1 not into Program Files folder.

0 件の賞賛
返信

7,883件の閲覧回数
richardtolleson
Contributor I

Ed,

Install into c drive not into program files?

Rick

0 件の賞賛
返信

7,883件の閲覧回数
kef2
Senior Contributor V

Rick,

Program Files in Win >=7 is special folder. When application installed in one of PF subfolderss tries to write some settings also to PF folder, windows redirects writing and reading of such data files to App Data \ Roaming folder. Some programs see this on-the-fly redirection well, and some not. CW5.1 seems having problems with this Win7 feature. So just install to c:\CW, or c:\Freescale\CW or whatever you may like, but not in to Program Files.

0 件の賞賛
返信

7,883件の閲覧回数
richardtolleson
Contributor I

Thanks James,

I will try it out and let you know.

Rick

0 件の賞賛
返信

7,883件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I recommend to install it into

c:\freescale\cw_5.1

Installing development tools into 'program files' will put it onto Windows special control which can have bad side effects.

0 件の賞賛
返信

7,883件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Richard,

is this problem solved?

on our side both of these two versions are installed on my computer. they are running well and no driver problem happens.

0 件の賞賛
返信

7,882件の閲覧回数
richardtolleson
Contributor I

This problem is not solved.

I did have both versions running at one time and then something happened, maybe an update or a gpo from the ITS group. But everything I look at shows normal?

0 件の賞賛
返信

7,882件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

We couldn't see your screenshot, please upload it again

0 件の賞賛
返信

7,882件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

please upload the error screenshot?

in device manger, the jungo driver appears normal?

0 件の賞賛
返信