What is the advantage of using the online (instead of offline) installer for CW?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the advantage of using the online (instead of offline) installer for CW?

ソリューションへジャンプ
1,040件の閲覧回数
lancefisher
Contributor III

I've tried both and it seems that while the initial download for the online version is significantly smaller, it ends up downloading more data overall so the result takes longer.  Also with the online version I think there are more frequent pauses for user input.  I'm working with a rather slow connection (0.5 to 1 MBPS) which makes the extra download particularly painful but at this time I can't see any reason to use the online method.

ラベル(1)
0 件の賞賛
返信
1 解決策
913件の閲覧回数
BlackNight
NXP Employee
NXP Employee

With the 'online' version it downloads the needed packages 'on demand'. I have not measured it, but I would think that if you install say just S08, than it might be faster. But generally I recommend to download the 'offline' version: that way you have downloaded everything and you can distribute it locally. At the end this worked for me best.I think the online version works best with a very fast internet connection. Mine is less than 2 MBit too.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
914件の閲覧回数
BlackNight
NXP Employee
NXP Employee

With the 'online' version it downloads the needed packages 'on demand'. I have not measured it, but I would think that if you install say just S08, than it might be faster. But generally I recommend to download the 'offline' version: that way you have downloaded everything and you can distribute it locally. At the end this worked for me best.I think the online version works best with a very fast internet connection. Mine is less than 2 MBit too.

0 件の賞賛
返信