jungo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

jungo

4,919 Views
richardtolleson
Contributor I

I am having trouble running 2 different versions of freescale software and keeping the jungo drivers working. I need to run cw_hc12_v5.1_special and cw_mcu_v10.1_se.

the 10.1 installs and runs perfect. v5.1 will install but it fails to load and run the jungo driver. it fails even if i am logged in as administrator, right click and "run as administrator",

virus scan is disabled, and it is removed from the domain.

I am running windows 7 enterprise.

Labels (1)
Tags (1)
0 Kudos
Reply
9 Replies

4,732 Views
kef2
Senior Contributor V

Richard, try installing CW5.1 not into Program Files folder.

0 Kudos
Reply

4,731 Views
richardtolleson
Contributor I

Ed,

Install into c drive not into program files?

Rick

0 Kudos
Reply

4,731 Views
kef2
Senior Contributor V

Rick,

Program Files in Win >=7 is special folder. When application installed in one of PF subfolderss tries to write some settings also to PF folder, windows redirects writing and reading of such data files to App Data \ Roaming folder. Some programs see this on-the-fly redirection well, and some not. CW5.1 seems having problems with this Win7 feature. So just install to c:\CW, or c:\Freescale\CW or whatever you may like, but not in to Program Files.

0 Kudos
Reply

4,731 Views
richardtolleson
Contributor I

Thanks James,

I will try it out and let you know.

Rick

0 Kudos
Reply

4,731 Views
BlackNight
NXP Employee
NXP Employee

I recommend to install it into

c:\freescale\cw_5.1

Installing development tools into 'program files' will put it onto Windows special control which can have bad side effects.

0 Kudos
Reply

4,731 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Richard,

is this problem solved?

on our side both of these two versions are installed on my computer. they are running well and no driver problem happens.

0 Kudos
Reply

4,730 Views
richardtolleson
Contributor I

This problem is not solved.

I did have both versions running at one time and then something happened, maybe an update or a gpo from the ITS group. But everything I look at shows normal?

0 Kudos
Reply

4,730 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

We couldn't see your screenshot, please upload it again

0 Kudos
Reply

4,730 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

please upload the error screenshot?

in device manger, the jungo driver appears normal?

0 Kudos
Reply