how can i obtain less period in pwm beam

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how can i obtain less period in pwm beam

跳至解决方案
1,979 次查看
andres
Contributor I
hi:
i'm trying to use into my  hcs08 GB60A, the pwm beam, in CW hc08 v5.1  but the max. frecuency is 2Khz(501us),it's the max. frecuency ? how i can obtain more than 2Khz frecuency (less than 501us)?  for example: 10Khz
 
thanks  
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,395 次查看
ProcessorExpert
Senior Contributor III
Dear Customer,
 
The max. frequency setting in the PWM bean is depended on GB60A clock setting among others. For the default cpu setting it is possible to use frequency higher than 2kHz (501us). Please check cpu clock setting.
 
Best Regards,
Jan Pospisilik, Processor Expert Support

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,396 次查看
ProcessorExpert
Senior Contributor III
Dear Customer,
 
The max. frequency setting in the PWM bean is depended on GB60A clock setting among others. For the default cpu setting it is possible to use frequency higher than 2kHz (501us). Please check cpu clock setting.
 
Best Regards,
Jan Pospisilik, Processor Expert Support
0 项奖励
回复