how can i obtain less period in pwm beam

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how can i obtain less period in pwm beam

ソリューションへジャンプ
1,968件の閲覧回数
andres
Contributor I
hi:
i'm trying to use into my  hcs08 GB60A, the pwm beam, in CW hc08 v5.1  but the max. frecuency is 2Khz(501us),it's the max. frecuency ? how i can obtain more than 2Khz frecuency (less than 501us)?  for example: 10Khz
 
thanks  
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,384件の閲覧回数
ProcessorExpert
Senior Contributor III
Dear Customer,
 
The max. frequency setting in the PWM bean is depended on GB60A clock setting among others. For the default cpu setting it is possible to use frequency higher than 2kHz (501us). Please check cpu clock setting.
 
Best Regards,
Jan Pospisilik, Processor Expert Support

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,385件の閲覧回数
ProcessorExpert
Senior Contributor III
Dear Customer,
 
The max. frequency setting in the PWM bean is depended on GB60A clock setting among others. For the default cpu setting it is possible to use frequency higher than 2kHz (501us). Please check cpu clock setting.
 
Best Regards,
Jan Pospisilik, Processor Expert Support
0 件の賞賛
返信