how can i obtain less period in pwm beam

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how can i obtain less period in pwm beam

Jump to solution
1,978 Views
andres
Contributor I
hi:
i'm trying to use into my  hcs08 GB60A, the pwm beam, in CW hc08 v5.1  but the max. frecuency is 2Khz(501us),it's the max. frecuency ? how i can obtain more than 2Khz frecuency (less than 501us)?  for example: 10Khz
 
thanks  
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,394 Views
ProcessorExpert
Senior Contributor III
Dear Customer,
 
The max. frequency setting in the PWM bean is depended on GB60A clock setting among others. For the default cpu setting it is possible to use frequency higher than 2kHz (501us). Please check cpu clock setting.
 
Best Regards,
Jan Pospisilik, Processor Expert Support

View solution in original post

0 Kudos
Reply
1 Reply
1,395 Views
ProcessorExpert
Senior Contributor III
Dear Customer,
 
The max. frequency setting in the PWM bean is depended on GB60A clock setting among others. For the default cpu setting it is possible to use frequency higher than 2kHz (501us). Please check cpu clock setting.
 
Best Regards,
Jan Pospisilik, Processor Expert Support
0 Kudos
Reply