headers not found

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

headers not found

1,436件の閲覧回数
Jim_P
Contributor III

using the S08JM16 for a project with CW 10.1 running on Windows 7 64 bit

 

I have different directories setup in the project file.  one for the application with the code in this directory.

a different directory for the real time monitor that I have developed and use as starting code for many projects.

 

this code in in the monitor_Lib directory.  and was drag and dropped into the monitor_lib directory and option to have the code linked into the project.

 

The headers for the different files are in the Standard CW header folder.

 

the problem is that while I can select and open the header files, the compiler can not seem to find the header files.

 

any suggestion

 

thanks

Jim P

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,343件の閲覧回数
CrasyCat
Specialist III

Hello

 

Did you add the path to the include files to your project?

 

CrasyCat

0 件の賞賛
返信