flash write and read/

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flash write and read/

1,535件の閲覧回数
guochunhua
Contributor II

Dear sir/ms.

I have made a program in codewarrior 10.7,the cpu is mc56f84789. In PE, I have met two problems, they are follows.

1. I have added a flash module in my program,but I can not read or write the flash correctly, can you give me an example that how I read or write the flash? It is wonderful if you can give me a video.

2. I have added eFlexPWM module, there is a fault in my program when the PWM fault pin is high level. If there is a fault, sometimes enter the fault interrupt,sometimes does not enter the fault interrupt, how can I set the fault pin to enter the fault interrupt ? or which options can I set to enter the fault interrupt? can you give me an example? It is wonderful if you can give me a video.

Best regards.

chunhua guo

0 件の賞賛
返信
1 返信

1,326件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Chunhua,

This is a duplicate question of

https://community.nxp.com/thread/469202 

We have support engineer already contacted you via that link.

Please have a look, if that's not clear, please contact the support engineer with reply.

BR

Jennie Zhang

0 件の賞賛
返信