developmet board for motor driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

developmet board for motor driver

2,466 Views
mansoorahmedk
Contributor I

Hi all,

          am new to this forum and also to free scale, am designing a motor driver of my own (BL DC)  kindly help me for this as which development board will meet my requirements to design. i have attached the pdf of my project requirement kindly please go through and reply me friends.

thank you in advance.

Labels (1)
0 Kudos
Reply
2 Replies

2,339 Views
trytohelp
NXP Employee
NXP Employee

Hi,

May be you can find other information on the Freescale web site.

We've a section for Motor Control.

Please have a look to this link:

      http://www.freescale.com/webapp/sps/site/homepage.jsp?code=MOTORCONTROLHOME&tid=vanMOTORCONTROL

Hope this will help you.


Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,339 Views
eduardo_viramon
NXP Employee
NXP Employee

Hi!

Currently the option Freescale offers as a motor control development platform is the TWR-MC-LV3PH motor control board. This is a low voltage motor control system based on the tower system:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-MC-LV3PH&tid=m32TWR

I would also recommend to you to use the new Kinetis KV10 as development MCU, it is ideal for simple low-cost motor control:

TWR-KV10Z32: Kinetis KV1x Family Tower System Module

Regards,

Eduardo V.

0 Kudos
Reply