command to assemble in a makefile:

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

command to assemble in a makefile:

跳至解决方案
1,786 次查看
raghav_sarma
Contributor I
Hallo,
 
I'm building my application by using make and not sure of the command to convert an assembly file, Do_On_Stack.asm, to an object file - Do_On_Stack.o using the assembler.
 
i.e. the command in the makefile will be something like:
 
Do_On_Stack.o : Do_On_Stack.asm
                       $(ASSEMBLER) XXXX
 
where: (ASSEMBLER) - is a variable pointing to the location of the assembler exe file ahc12.exe and XXX are the instructions that I'm looking for.
 
What is this command and what arguments, options must be given to the assembler? I'm using the cygwin shell which attempts to provide unix like functionality on a Windows machine.
 
Raghav
 
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,073 次查看
CompilerGuru
NXP Employee
NXP Employee
Have a look in any assmebly HC12 project in the CW ide, there in the compiler/linker/assembler settings is a checkbox "show command line" (or similar) which dumps the complete command line used by this tool to the message window.
Note that the content of the message window can be copied with ctrl-c.
Of course you don't need all the options as used in CW, for example it passes to many access paths to the tools.

Daniel

PS: If you do not have a project, create one with the wizard.

BTW. the tools support both UNIX style / and dos style \ directory separators. I always had problems with the dos style because cygwin's sh treats them as escape character, so best if you work only with UNIX style paths.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,074 次查看
CompilerGuru
NXP Employee
NXP Employee
Have a look in any assmebly HC12 project in the CW ide, there in the compiler/linker/assembler settings is a checkbox "show command line" (or similar) which dumps the complete command line used by this tool to the message window.
Note that the content of the message window can be copied with ctrl-c.
Of course you don't need all the options as used in CW, for example it passes to many access paths to the tools.

Daniel

PS: If you do not have a project, create one with the wizard.

BTW. the tools support both UNIX style / and dos style \ directory separators. I always had problems with the dos style because cygwin's sh treats them as escape character, so best if you work only with UNIX style paths.
0 项奖励
回复