code generation error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

code generation error

ソリューションへジャンプ
3,326件の閲覧回数
ara_mike
Contributor I
CodeWarrior HCS12 v4.6
using CpuMC9S12NE64CFU
 
When i add a PulseAccumulator using the Processor Expert i get an error during code generation
 
INTERNAL ERROR at line 40: Unexpected status, please contact our support department (file: Drivers\CommonReginitialization.prg)
 
Any suggestions??
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,374件の閲覧回数
CrasyCat
Specialist III

Hello

 

This seems to be a completely different issue.

 

Please post a new message on the "CodeWarrior for 56xxx DSC" and provide more information on the problem you are facing.

 

Alternatively you can submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,374件の閲覧回数
admin
Specialist II

I'm encountering the same problem. Actually I want to migrate my project from CW 8.2.3 to 8.3.

But when I try to build my project in CW 8.3 This error appears.

 

CPU: 56F8037.

 

Would you please guide me through this?

0 件の賞賛
返信
2,375件の閲覧回数
CrasyCat
Specialist III

Hello

 

This seems to be a completely different issue.

 

Please post a new message on the "CodeWarrior for 56xxx DSC" and provide more information on the problem you are facing.

 

Alternatively you can submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.

 

CrasyCat

0 件の賞賛
返信
2,374件の閲覧回数
ProcessorExpert
Senior Contributor III
We need more information in order to evaluate the problem. What version of Processor expert are you using? Could you please provide us a project demonstrating this error?

Information how to find out the version of the currently installed Processor Expert can be found here: http://www.processorexpert.com/lnk_mcfaq_HCS12.php


Processor Expert Support Team
www.processorexpert.com
0 件の賞賛
返信