code generation error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

code generation error

Jump to solution
3,414 Views
ara_mike
Contributor I
CodeWarrior HCS12 v4.6
using CpuMC9S12NE64CFU
 
When i add a PulseAccumulator using the Processor Expert i get an error during code generation
 
INTERNAL ERROR at line 40: Unexpected status, please contact our support department (file: Drivers\CommonReginitialization.prg)
 
Any suggestions??
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,462 Views
CrasyCat
Specialist III

Hello

 

This seems to be a completely different issue.

 

Please post a new message on the "CodeWarrior for 56xxx DSC" and provide more information on the problem you are facing.

 

Alternatively you can submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.

 

CrasyCat

View solution in original post

0 Kudos
Reply
3 Replies
2,462 Views
admin
Specialist II

I'm encountering the same problem. Actually I want to migrate my project from CW 8.2.3 to 8.3.

But when I try to build my project in CW 8.3 This error appears.

 

CPU: 56F8037.

 

Would you please guide me through this?

0 Kudos
Reply
2,463 Views
CrasyCat
Specialist III

Hello

 

This seems to be a completely different issue.

 

Please post a new message on the "CodeWarrior for 56xxx DSC" and provide more information on the problem you are facing.

 

Alternatively you can submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.

 

CrasyCat

0 Kudos
Reply
2,462 Views
ProcessorExpert
Senior Contributor III
We need more information in order to evaluate the problem. What version of Processor expert are you using? Could you please provide us a project demonstrating this error?

Information how to find out the version of the currently installed Processor Expert can be found here: http://www.processorexpert.com/lnk_mcfaq_HCS12.php


Processor Expert Support Team
www.processorexpert.com
0 Kudos
Reply