choosing the right code development studio for MCS9S12XDT256CAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

choosing the right code development studio for MCS9S12XDT256CAG

3,498 Views
yaprak
Contributor I

Hi,

 

I'm using the chip MC9S12XDT256CAG. It is the HCS12 series with 256K flash memory and I need to buy a software licence for it. I've searched in the website for the suitable licence. I gave the link below:

 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-SUITE-STANDARD&tab=Buy_Parametric_...

 

I looked about the meanings of the licences. There is somthing that I do not understand, on the list of licences. I write my question below:

 

for example :

 

CWA-BAS2STD-FL

 

CWA: means annual licence

FL: means floating licence. All of the computers connected to a server can run the computers. 

BAS2STD: means from basic to standart licence upgradable.

 

What should I understand about licence that is upgradable from basic to standart? I'm buying a licence for the first time and I'm planning to buy a standart licence. If I buy this licence does it mean that I can use this licence both for the basic one and the standart one?

 

Can you help me about this problem please?

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

2,384 Views
J2MEJediMaster
Specialist I

If you upgrade the license from basic to standard, the standard license replaces the basic one.

 

---Tom

 

0 Kudos
Reply

2,384 Views
yaprak
Contributor I

If I'm buying for the first time can I use this licence?

 

I'm confused

0 Kudos
Reply

2,384 Views
Sten
Contributor IV

Hi yaprak

 

I think you have to buy a CW?-STANDARD_?L-license (CWP or CWA and FL or NL). The BA2STD is just a upgrade from BASIC to STANDARD and probably requires that you have earlier bought a BASIC-license.

 

Sten

 

0 Kudos
Reply

2,384 Views
CrasyCat
Specialist III

Hello

 

The standard edition license includes all features from Basic license plus the standard edition specific features.

 

 

CrasyCat

0 Kudos
Reply