any comments on assembler directive (PLEN) ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

any comments on assembler directive (PLEN) ?

2,933 Views
klem
Contributor II
0 Kudos
Reply
5 Replies

2,653 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Bob,

I ever answered you under https://community.nxp.com/thread/445093 

Can you please check it?

any question with it?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,653 Views
klem
Contributor II

Hi Jennie I use CW 6.1 for HC(s)08 assembler, When I use PLEN 50 (for example)

my .list file page length is still 65 lines (default page length) The listing shows the form feed after

line 65.My assembler takes the directive OK with out failure so I assume I enter it OK.

I would like to use shorter page length, say 30 or so to print some listing in landscape mode.

Any suggestions

Bob

0 Kudos
Reply

2,653 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Bob,

I just tested PLEN with CW for HCS08 v6.1.

I set PLEN as 50. I can get the right line number in a page in list file.

so I can't reproduce your problem.

to investigate your problem further, I need:

1. a video to show me your problem

2. your project.

I need test it directly from my side.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,653 Views
klem
Contributor II

Hi  Jennie,

I finally got "plen" to work. This  works for me but makes absolutely no sense..

If I put the PLEN command AFTER any 'include' statement, the set page length

works just fine. I have not tried putting an 'include' statement after a 'PLEN' to see

if the include cancels the PLEN . Right now I have printer problem to solve first.

Thanks for your interest. I will let you know if I find anything else.

Bob W

0 Kudos
Reply

2,653 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bob,

Could you pleas describe your question detail ?

Which chip ? Which version of CW ? What about the problem ?

BR

Alice

0 Kudos
Reply